Settings tab
Figure 5-7: Settings tab with Firmware tab
The Settings tab is used to:
- View and update the firmware for the KAS Runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running. - Change the date or time in the Date/Time tab.
- View the network settings and modify the IP address.
- See Network tab.
- Reset the Controller to Factory Settings
- Reset the controller to factory settings.
- AKD PDMM and PCMM: Access the SD Card Actions.
- PCMM2G: Use the USB Flash Drive tab for a USB flash drive.
- Access the Change the Web server's User Account Password to change the password.