Plugging Probes, Mapping Variables
These types of variables can be mapped:
- Pipe Block variable
- IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 variable, which is any other variable. - PLCopen
A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML axis values.
You can connect a probe to a variable in one of these ways:
- From the Softscope, see Mapping a Variable to the Oscilloscope.
- From the Dictionary, see Plug a Probe from the Dictionary.
- From the Pipe Network, see Plugging a probe from the Pipe Network.