Smart Feedback Adapter (SFA)
Kollmorgen provides an optional Smart Feedback Adapter (SFA) to allow feedback devices that normally connect to X23 (FB3) to connect through X1 (FB1), X2 (FB2) and X5 (FB2) instead. For example, on a dual axis drive requiring two resolver feedbacks, X23 could be used for one feedback and an SFA on X2 could be used for the other feedback. See Feedback Connector X41 for details on connecting SFA hardware to AKD2G.
For connections that support SFA (X1, X2 and X5), SFA feedback types can be selected using FB#.SELECT in the same manner as other feedbacks. If they are plug-and-play, FB#.SELECT can be set to -1 to auto-identify them. SFA feedback types appear as options for FB#.SELECT when the corresponding feedback connector supports SFA. For example, FB1.SELECT and FB2.SELECT show the SFA feedback types as options. See FB#.SELECT for a list of supported SFA feedback.
When the feedback is selected (see FB#.SELECT), the SFA is programmed with an FPGA
"Field-Programmable Gate Array"
FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable" image automatically if needed.
SFA cable flying leads connected to X1 (FB1, EEO3) or X2/X5 (FB2, EEO4):
|
|
|
Jump to a section about Feedback:
- Feedback Views
- Feedback Configuration
- Feedback Methods
- Smart Feedback Adapter (SFA)
- Non-Plug and Play Feedback Devices