Function Block Diagram (FBD) Editor
"Function Block Diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks Editor is a graphic tool used to enter and manage Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. Diagrams according to the IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 standard.
- The editor supports advanced graphic features such as drag-and-drop, object resizing, and connection line routing features to rapidly and freely arrange the elements of a diagram.
- Insert in an FBD diagram graphic elements of the FFLD
"Free Form Ladder Diagram" (Ladder Diagram) language (e.g., contacts and coils).
|
FBD Diagram Components |
Related Sections |
|---|---|
|
Selecting and entering variables and FB instances
|
|
|
FFLD Components |
|
|
|
-
-
When a contact or a coil is selected, press the Spacebar to change its type (e.g., normal, negated, pulse).
Boolean connections can be negative at the entry of a block.
Execution order can be displayed.