MLMotionStop
Function - Stops the motion bus driver, motion engine, and EtherCAT network operation, resulting in the EtherCAT network transitioning to the Init state.
Inputs
-
- There are no Inputs for this function / function block.
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE after requesting all bus drivers to stop. See Function - General Rules. |
Remarks
- Results in the EtherCAT network transitioning to the Init state.
- Returns TRUE if the function succeeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Stop the EtherCAT network
ON StopMotionEngine DO
MLMotionStop();
END_DO;
See Also