MC_ResetError

PLCopen motion icon

 Function - Resets the errors of the specified axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

En

BOOL

FALSE, TRUE

N/A

No default

Requests to reset the axis errors.

Axis

AXIS_REF

1 to 256

N/A

No default

Name of a declared instance of the AXIS_REF library function.

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Function block executed successfully.

See Function - General Rules.

Remarks

  • Makes the transition from the state ErrorStop to StandStill by resetting all internal axis-related errors and clearing pending commands.
  • This does not affect the output of the FB instances.

This function performs these tasks in sequence:

  1. Sends a request to the drive to clear any drive faults that exists
  2. Resets the axis errors

  • The condition causing the axis error has to be corrected before calling this function. The axis error still remains until the error condition exists when this function is called.

See Transition Events and Actions, #15 in the status machine of the CANopen protocol.

Figure 1: MC_ResetError

FBD Language Example

Not available.

FFLD Language Example

IL Language Example

Not available.

ST Language Example

            //reset the axis and drive errors for Axis 1
            
MC_ResetError( Axis1 );