MLBlkReadModPos

Pipe Network motion icon

 Function - Gets the value of the period of a block in user units.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

-2147483648 to 2147483647

N/A

No default

ID number of a created Pipe Block.

Outputs

Output

Data Type

Range

Unit

Description

ModuloPosition

LREAL

 

User units

Current period value for selected Pipe Block.

Remarks

  • The output value of a block is reset each time it reaches its period value.

Figure 1: Modulo position of the axis.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Return and save the Period of a Pipe Block 
GearPeriod := MLBlkReadModPos( PipeNetwork.MyGear );

See Also