MLBlkWriteModPos
Function - Sets the value of the period of a block in user units.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
|
ModuloPosition |
LREAL |
No range |
User units |
No default |
Designated new Period Value for selected Pipe Block. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
|
Returns TRUE if the function block is executed. See Function - General Rules. |
Remarks
- The output value of a block is reset each time it reaches its period value.
Figure 1: Modulo position of the axis.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Set the Period of a Pipe Block to 300
MLBlkWriteModPos( PipeNetwork.MyGear, 300 );
See Also