MLPmpWriteJerk
Function - Sets the Jerk parameter of a PMP block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a PMP function block in the Pipe Network. |
|
Jerk |
LREAL |
> 0 (zero) |
User unit/sec3 |
No default |
Jerk value. The value is entered in the JERK field in the Parameter tab. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE if the function or function block is successfully executing. See Function - General Rules. |
Remarks
- Can be set when adding a PMP block to a Pipe Network and defining the parameters for that block.
- Returns TRUE if the function succeeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLPmpWriteJerk( PipeNetwork.PmpMaster, 15.0 ) ;
See Also