MLTrigReadDelay
Function - Returns the time the trigger block uses to compensate the delay of the sensor that captures the triggering signal.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
Identifier of the trigger block. |
|
En |
BOOL |
No range |
N/A |
No default |
Enables execution. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Delay |
LREAL |
No range |
Microseconds |
Value of the delay compensation currently applied by the trigger block. |
|
OK |
BOOL |
No range |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
- Returns the delay programmed in a trigger block by the MLTrigWriteDelay function to compensate for the reaction time required by the sensor.
- Electronic sensors are not able to respond immediately to a signal.
- Sensors usually require a certain amount of time to process a change of state in their input signal.
Fast Homing - Inputs
See these topics for more information:
- Fast Homing Example with the Pipe Network Motion Engine Axis Pipe Block
- Fast Homing Example with the PLCopen Motion Engine
- Fast Inputs with Pipe Network Motion
- Pipe Network Registration and Fast Homing
- Registration Position Capture Example with Pipe Network Trigger Block
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also