SigID

PLCopen motion icon

 Function - Get the identifier of a Signal resource.

Inputs

Input

Data Type

Range

Unit

Default

Description

SIGNAL

STRING

 

 

 

Name of the signal resource.

Must be a constant value.

COL

STRING

 

 

 

Name of the column within the signal resource.

Must be a constant value.

Outputs

Output

Data Type

Range

Unit

Description

ID

DINT

 

 

ID of the signal to be passed to other blocks.

Remarks

  • Some blocks have arguments that refer to a signal resource.
    • For all these blocks, the signal argument is materialized by a numerical identifier.

FBD Language Example

FFLD Language Example

IL Language Example

Op1: LD    'MySignal'
     SigID 'FirstColumn'
     ST ID

ST Language Example

ID := SigID ('MySignal', 'FirstColumn');

See Also