SigScale

PLCopen motion icon

 Function - Get a point from a Signal resource.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

 

 

 

ID of the signal resource, provided by the SigID function.

TIME

TIME

 

 

 

Time (X) coordinate of the point within the signal resource.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL

 

 

Value (Y) coordinate of the point in the signal.

Remarks

  • The ID argument is the identifier of the signal resource.
    • Use the SigID function to get this value.
  • This function:
    • Converts a time value to an analog value as defined in the signal resource.
    • Can be used instead of the SigPlay function block to trigger the signal using a specific timer.

FBD Language Example

FFLD Language Example

IL Language Example

Op1: LD     IN
SigScale ID
ST       Q

ST Language Example

Q := SigScale (ID, IN);

See Also