AXIS#.BODE.EXCITEGAP
Description
AXIS#.BODE.EXCITEGAP controls how often the excitation is updated. The excitation is updated every n drive samples, where n is AXIS#.BODE.EXCITEGAP. For example, if AXIS#.BODE.EXCITEGAP = 2, then the excitation is updated every 2/(16,000 Hz) = 1/8,000 Hz = 0.000125 sec. When measuring a system, update the excitation only as often as the data is recorded.
Example
Set excitation update rate to 8,000 Hz:
--> AXIS1.BODE.EXCITEGAP 2
Set excitation update rate to 4,000 Hz:
--> AXIS1.BODE.EXCITEGAP 4
Get excitation update rate (already set to 8000 Hz):
--> AXIS1.BODE.EXCITEGAP 2
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Drive samples |
|
Range |
1 to 255 drive samples |
|
Default Value |
2 drive samples |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics
Using the Performance Servo Tuner | Using the Performance Servo Tuner: Advanced