PL.FBSOURCE

Description

This parameter determines the feedback source that the position loop uses. A value of 0 for this parameter selects the primary feedback, a value of 1 selects the secondary feedback. If you use the secondary feedback as the source for the position loop, then FB2.MODE mode should be set as 0 (A/B signals). A/B signals are the only supported feedback type as secondary feedback into the position loop. Other settings for FB2.MODE are intended as pulse inputs or a gearing command when PL.FBSOURCE remains 0.

Value Description
0

Primary Feedback connected to X10.

1 Secondary Feedback (DRV.HANDWHEEL) connected to X7 or X9.
2 Tertiary Feedback connected to X9 (only supported with AKD-x-xxxxx-NBxx-xxxx).

General Information

Type

NV Parameter

Units

N/A

Range

Range will differ depending on drive model.
0 to 1 (for AKD-x-xxxxx-NAxx-xxxx)
0 to 2 (for AKD-x-xxxxx-NBxx-xxxx)

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5128h/0

M_01-00-00-000

Related Topics

PL.ERR | PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop