PL.KI

Description

PL.KI sets the integral gain of the position regulator PID loop.

General Information

Type

NV Parameter

Units

Hz

Range

0 to 250 Hz

Default Value

0 Hz

Data Type

Float

See Also

PL.KP, PL.KD

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3480h/0 M_01-00-00-000

Related Topics

PL.ERR | PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop