Programming Languages

This section provides information about the syntax, structure, and use of declarations and statements supported by the KAS-IDE application language.

These are the available programming languages of the IEC 61131-3 standard:

A language must be selected for each program or User-Defined Function Block of the application.

See these pages about the IEC 61131-3 programming languages: