ECATWCStatus
Function - Returns the current number of working counter errors for the Sync unit.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
SyncUnit |
INT |
-32768 to +32767 |
N/A |
No default |
Sync Unit Index |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Count |
UDINT |
No range |
N/A |
Working Counter error. |
Remarks
- The working counter errors are cleared to zero when the EtherCAT network is taken from Init to OP state.
- Value 0 (zero)means no working counter errors.
- When the value is non zero, the master automatically reduces the count by 1 for every thousand good frames received.
- When the working counter error exceeds the Working Counter Error Limit, the EtherCAT network is stopped.
-
- See Check for Working Counter Errors in Example: EtherCAT Communication Diagnosis Steps for an example of implementing this function.
Figure 1: ECATWCStatus
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(********************************************************)
(* read Ethercat Working counter value *)
(********************************************************)
wcErrorCounter := ECATWCStatus( 0 );
See Also