MC_CamOut

PLCopen motion icon

 Function Block - Disengages the slave axis from an MC_CamIn move or the master axis immediately in a cam block.

Inputs

Input

Data Type

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, request to queue the move.

Slave

AXIS_REF

1 to 256

N/A

No default

Name of a declared instance of the AXIS_REF library function.

Acceleration

LREAL

No range

User unit/sec2

No default

Trapezoidal: Acceleration rate.

S-curve: Maximum acceleration.

See S-curve and Trapezoidal Acceleration / Deceleration.

Deceleration

LREAL

No range

User unit/sec2

No default

Trapezoidal: Deceleration rate.

S-curve: Unused.

See S-curve and Trapezoidal Acceleration / Deceleration.

Jerk

LREAL

No range

User unit/sec3

No default

Trapezoidal: 0 (zero).

S-curve: Constant jerk.

See S-curve and Trapezoidal Acceleration / Deceleration.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

Indicates the axis is disengaged from its master.

Busy

BOOL

FALSE, TRUE

N/A

Indicates this function block is executing.

Active

BOOL

FALSE, TRUE

N/A

Indicates this move is the Active move.

CommandAborted

BOOL

FALSE, TRUE

N/A

Indicates the move was aborted.

Error

BOOL

FALSE, TRUE

N/A

Indicates either:

  • An invalid input was specified.
  • No MC_CamIn move was active.

ErrorID

INT

No range

N/A

When the Error output is:

  • high, this output indicates the type of error.
  • low, this output is undefined.

See PLCopen Function Block ErrorIDs.

Remarks

  • See Function Blocks - General Rules about how inputs and outputs work.
  • If this function block is called and the active move is not a MC_CamIn move, this function block returns an error and the active move is not aborted.
  • This function block:
    • Aborts the active MC_CamIn move.
    • Disengages the axis from its master.
    • Disengages the slave axis from a MC_CamIn move.
    • Commands the axis to continue at its current velocity.
      • The axis continues to run at this velocity until this MC_CamOut move is aborted.

  • The current velocity is calculated by taking the average of the actual velocity during the previous 16 cycles.

Cancel the Cam Motion

  • An alternative method to cancel the cam motion is a single axis move (MC_MoveAbsolute, MC_MoveRelative, MC_MoveAdditive, MC_MoveVelocity, and MC_Halt) with the BufferMode input set to 0 (zero).
    • This cancels the MC_CamIn function and starts the new motion function on the slave axis.
  • Many applications prefer calling MC_Halt instead of MC_CamOut because it does not send a velocity command to the slave axis.

Figure 1: MC_CamOut

FBD Language Example

Not available.

FFLD Language Example

IL Language Example

Not available.

ST Language Example

(* MC_CamOut ST example *)
Inst_MC_CamOut(ExecCamOut1,Axis1,CamOut1Acc,CamOut1Dec,CamOut1Jerk);
//Inst_MC_CamOut is an instance of MC_CamOut

See Also