MLAxisGenWriteSpd
Function - Sets the speed of the internal generator of an axis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
AxisID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
|
Speed |
LREAL |
No range |
User unit/sec |
No default |
Sets the generator Speed value. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
Remarks
This function or function block does not generate any motion.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisGenWriteSpd(PipeNetwork.Axis1, 500 ) ;
See Also