MLCNVConnectEx
Function - Connects the output of a pipe to an axis data other than the control position.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Converter object. |
|
AxisID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Axis object. |
|
ValueID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
Specify this constant:
|
|
ValueInfo |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
This value is ignored. It must be set to 0 (zero). |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE if the converter is connected to the Axis object. See Function - General Rules. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
- This function:
- Connects an extra converter Pipe Block to the specified axis.
- Connects several converter Pipe Blocks to the same axis and acts on different data.
- Normally a Converter block sends position values to an Axis.
-
-
This FB does NOT work if you have Simulated the device.
In this instance, the FB continuously generates error messages in the Controller log window.
-
-
Add 16#8000 to the designated IDN number for ValueID input. 8000 in hexadecimal signals a vendor-specific IDN value.
- The PDO values are overwritten by Mapped PLC variables including either:
- A possible link to the mapping of variables.
- The section on MLParamWrite() warning indicating that the function block write of Analog output is overwritten by the MLCnvConnectEx function.
Precedence Rules
- A PLC variable mapped to Analog Output takes precedence.
- If MLCNVConnect assigns a Pipe output to an Analog Output, it takes precedence over a DriveParamWrite function call.
- DriveParamWrite modifies the Analog Output but is overwritten by the higher precedent options if they are present.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Connect a converter Pipe Block named “CNV1” to the pipe block named AXIS1, And send feed-forward (EC_ADDITIVE_TORQUE_VALUE) to the drive
MLCNVConnectEx( PipeNetwork.CNV1, PipeNetwork.AXIS1, EC_ADDITIVE_TORQUE_VALUE, 0 );
See Also