Sampler
|
Name |
Description |
|
Connects a sampler block to the specified CoE object in a PDO. |
|
|
Connects a sampler block to a pipe network axis or pipe block. |
|
|
Connects a sampler block to a specific PLCopen axis variable. |
|
|
Connects a sampler block to a specific Pipe Network axis variable. |
|
|
Initializes a sampler object. |
-
-
There is a delay when using an external encoder.
The delay is five cycles:
2 cycles to read the encoder from the AKD via EtherCAT,
1 cycle for computing,
2 cycles for sending the new position set point to the AKD).
This lag error is speed proportional (5 cycles * speed).
A Phaser block can be used to compensate for this lag.