Motion / Pipe Network
The KAS-IDE function library contains Motion Library (ML) function blocks (FBs) used to integrate motion from a Pipe Network in a PLC program.
These are the ML function blocks:
|
Function |
Description |
||
|
Block |
Manage the blocks: Create / activate. See Block for more information. |
||
|
Motion |
Prepare the physical motion part: init, reset, start, stop. See click here... for more information. |
||
|
Pipe Block |
Manage each specific Pipe Block: Read / write parameters. The function blocks are: |
||
|
Pipe Network |
Manage the Pipe Network: Create / activate. See click here... for more information. |
-
-
Pipe Network code is generated automatically by the compiler.
Do not try to modify it.