Oscilloscope Graphical Area

The graph displays a subset of the collected data: the time-frame.

Figure 1: Example of the traces generated in the Oscilloscope.

The graph has these features to view and analyze the data:

  • Graduations are displayed on the left and lower sides of the graph.
  • Information concerning the time-frame of the graph and the amplitude of channels also appears at the bottom of the graph.
    • The current channel amplitude is underlined and the coordinates of the nearest collected sample are displayed.
  • It is possible to zoom in the graph using various methods.
  • It is possible to move the contents of the graph within the time-base.
  • See Trace Zoom Feature.

  • Moving the contents is possible only when the acquisition is stopped.

See Export the Oscilloscope Data for capturing the trace data.