Feedback_Status
Feedback_Status
|
Address: |
10274 (2822H) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Type: | Unsigned16 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Access: |
Read Only |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Unit: |
N/A | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Range: | Unsigned16 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Default Value: | N/A | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Store Supported: |
No |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Description: |
This object returns some important information about the Feedback status. This object is managed at bit and the following tables show the meaning of each bits.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Notes: |
|