MT.MTNEXT

Description

MT.MTNEXT specifies the number of the following motion task and is used by the MT.SET and MT.LOAD command. This parameter is a temporary value. A motion task is only set after an MT.SET command.

The motion task control word can be selected so that a following motion task is executed after a first motion task. This parameter displays which motion task should be started after the first motion task.

General Information

Type

R/W Parameter

Units

N/A

Range

0 to 128

Default Value

0

Data Type

Integer

See Also

MT.NUM, MT.P, MT.V, MT.CNTL, MT.ACC, MT.DEC, MT.TNUM, MT.TNEXT, MT.SET , MT.LOAD

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

35BCh/0

M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2273 Byte No
Sercos® III 2 Octets
EtherNet/IP]
Instance Data Size Data Type
274 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

546

No 8 bit No M_01-03-00-000

Related Topics

Motion Tasks