Feedback Devices View

This view provides up-to-date data about the devices. Clicking on the feedback number field opens a Feedback # View to configure it.

Element Description Parameter
X# Indicates the connector used for the feedback  
Feedback # block [number] Identifies the feedback and serves as a link to the configuration view  
Type Indicates the feedback type identified FB#.IDENTIFIED
Actual Encoder Resolution

This parameter reports the actual encoder resolution of the feedback device. The drive calculates the FB#.RES value based on the encoder characteristics. It is provided in encoder counts/rev for rotary encoders and encoder counts/mm for linear encoders.

FB#.RES
Position Current position in raw feedback counts FB#.P
Graphical Indicator Visually indicates the position of the feedback within one revolution  
  FB Usage Indicates how the feedback is being used by an axis. Clicking an entry will open the view configuration.