MC_SetOverride
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BOOL |
0, 1 |
N/A |
No default |
Request to write the override factors. |
|
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances..
|
VelFactor |
REAL |
0.0, 2.0 |
N/A |
No default |
Velocity override factor. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Enabled |
BOOL |
|
|
Indicates the override values have been written. |
Busy |
BOOL |
|
|
Indicates this function block is executing. |
Error |
BOOL |
|
|
Indicates an invalid input was specified. |
ErrorID |
INT |
|
|
Indicates the error if Error output is TRUE. |
Remarks
- See Function Blocks - General Rules about how inputs and outputs work.
- A change in the velocity override factor takes effect immediately on the active move.
- The velocity override factor is applied to the programmed The act of performing a sequence of instructions or commands. velocity (of a MC_MoveAbsolute, MC_MoveAdditive, MC_MoveRelative, MC_MoveSuperimp, or MC_MoveVelocity function block) to determine the command velocity:
command velocity = programmed velocity * VelFactor
Figure 1: MC_SetOverride
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_SetOverride ST example *)
VelFactor := 1.25 ; //set the velocity factor to 1.25 (125%)
Inst_MC_SetOverride( TRUE , Axis1, VelFactor ); // Inst_MC_Setoverride is an instance of MC_SetOverride