Basic Operations

Data Manipulation

These are the language features for basic data manipulation:

Control Program Execution

Language Features

These are the language features to control program execution:

Structured Statements

These are the structured statements to control program execution:

Statement

Description

CASE  OF  ELSE  END_CASE

Switch to one of various possible statements.

EXIT

Exit from a loop instruction.

FOR  TO  BY  END_FOR

Execute iterations of statements.

IF  THEN  ELSE  ELSIF  END_IF

Conditional execution of statements.

ON

Conditional execution of statements.

REPEAT  UNTIL  END_REPEAT

Repeat a list of statements.

WAIT and WAIT_TIME

Suspends the execution of an ST program.

WHILE  DO  END_WHILE

Repeat a list of statements while a condition is TRUE.