RxPDO - KLD Drive CANopen Objects
This table identifies:
- The CANopen objects required by the motion engine and function blocks.
- Whether the objects are available in the default PDO.
- Their corresponding drive parameter.
-
-
Review the table to verify the objects needed by the features the application uses are included in the PDO selection.
|
RxPDO - KLD Drive CANopen Objects |
|||||
|---|---|---|---|---|---|
|
Index - subindex |
Object Name |
Required |
Associated ML FB |
Associated MC FB |
Associated Drive Parameter |
|
0x3780:1 |
AIN1.VALUE |
No |
N/A |
N/A |
|
|
0x3601:1 |
Physical Outputs Used by Onboard I/O mappings |
No |
N/A |
N/A |
DOUT.STATES |
|
0x6040:0 |
Yes |
Needed for motion engine axis to work properly |
|
|
|
|
0x6070A:0 |
Target Position |
Yes |
|
|
|
|
0x60B8:0 |
Touchprobe Function |
Yes |
|
|
|