Use Motion Function Block for Pipe Network
Use motion library function blocks in your PLC application program to interface to the Pipe Network (see Design Motion with Pipe Network).
ML function blocks are used to:
- Create and initialize the Pipe Network.
- Perform motion at a single-axis or multi-axis level.
- Read information from points in the Pipe Network.
Example:
- Read a high-speed input position from a Trigger Pipe Block.
- Read Command or Reference position from an Axis Pipe Block.
- Determine when a position has been reached in a Comparator Pipe Block.
- Modify how the blocks work in the Pipe Network.
Example:
- Change the phase offset of Phaser Pipe Block.
- Change the amplitude or offset of a CAM Profile.
- Change the speed of a Master Pipe Block.
Buffer Mode
With the Pipe Network engine, when a motion function block is executed while another one is presently executing, there is an immediate change.
That means the previous function block is aborted and the new one immediately becomes the active move and begins executing.
Motion Init
During initialization, and using the MLMotionInit function, the IEC 61131-3 application can create the different motion objects it needs (pipes, blocks, axes):
- Pipe Create
- Profile Create
-
-
When the state machine leaves the Init state, the creation of new motion objects is no longer allowed.
This is to avoid memory allocation problems while running the application.
Motion Start
- The Start method (MLMotionStart function) initializes the motion engine, motion bus driver, and initializes the EtherCAT network to operational mode.
- MLMotionStopbus driver deactivates the execution of the motion engine.
- The function blocks MLMotionStart, MLMotionStop, and MLMotionRstErr can be used by the IEC 61131-3 applications to navigate between states (i.e., Not initialized, Running, Stopped and Error).
Using the Q Output of ML Function Blocks for the Pipe Network
There is a Q output on most ML function blocks.
- The operation of the Q output is different for different ML function blocks.
- The Q output can be useful in PLC application programs.
Examples:
- MLAxisRel.Q is set when function block successfully executes.
- MLAxisStop.Q is set when motion is stopped (zero speed).
- MLPrfWriteIOffset.Q is set if cam offset has been changed to the new value.
See Also