You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Web Server KAS Application

KAS Application

This tab allows you to:

Item Description
Version of KAS App This label provides information about the name and version number of the application that is in the controller. The format is <project_name>:<version>.
The application's source code may be downloaded to the local computer if it is present on the controller. This is accomplished by clicking on the download icon (). This icon is found by the name and version information and is only present when source code is available.
Status of KAS App The state of the application, Started or Stopped.
Start Default mode (warm start) where the Retain Variables are loaded at the application startup. They are Not re-initialized; whereas other variables are started with their initial values.
Cold Start Use retain variables with their default values. Such starts occurs from time to time but are few.
Stop Stop the application
Auto-start

Select this option to automatically start the KAS application when the controller is powered up. The application will start using retained variables (a "warm start") after the controller has booted up.

To change this setting, click the Auto-start checkbox to either activate or deactivate this option and click the Apply button. The control will use the new setting at the next power-up. This option is recommended when the system is in production.

Clear all errors Clicking this button will clear the error log for all axes.

 

Axis

Log Configuration

Log Data

User Data

Shared Directory


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™