Functions sorted in alphabetical order:
| Name | Description | Return type |
|---|---|---|
|
Performs a move to an absolute position |
BOOL |
|
|
Performs an additive move relative for a specified distance from the endpoint of the previous move |
BOOL |
|
|
Returns the motion bus address of the axis |
DINT |
|
|
BOOL |
||
|
BOOL |
||
|
Returns the reference position of the axis |
None |
|
|
Creates a new axis object |
None |
|
|
None |
||
|
Enables or disables the internal TMP"Trapezoidal Motion Profile" This pipe block is a source block that frequently serves as a virtual master for a system composed of several pipes. Generally, a trapezoidal motion profile generator is used to generate a flow of values with a first derivative which produces a trapezoidal trajectory generator of the axis |
BOOL |
|
|
Checks if the internal TMP generator of the axis is enabled |
BOOL |
|
|
Checks if an axis is ready |
BOOL |
|
|
Returns the generator position of the axis |
None |
|
|
Gets the acceleration of the internal generator of an axis |
None |
|
|
Gets the deceleration of the internal generator of an axis |
None |
|
|
Gets the speed of the internal generator of an axis |
None |
|
|
Sets the acceleration of the internal generator of an axis |
BOOL |
|
|
Sets the deceleration of the internal generator of an axis |
BOOL |
|
|
Sets the speed of the internal generator of an axis |
BOOL |
|
|
Initializes an axis object |
BOOL |
|
|
Checks if a pipe is currently connected to the axis |
BOOL |
|
|
Checks if the axis got a trigger event |
BOOL |
|
|
Jogs at the specified speed |
BOOL |
|
|
Returns the pipe position of the axis |
None |
|
|
Powers up the axis. Enables Axis Servo DriveA servo drive is a special electric amplifier used to power electric servo motors. It monitors feedback signals from the motor and continually adjusts for deviation from expected behavior. |
BOOL |
|
|
Returns the adjustment of position done by the last power on to avoid bumps |
None |
|
|
Sets rated motor torque |
BOOL |
|
|
Read secondary feedback |
None |
|
|
Returns the actual position of the axis |
None |
|
|
Gets the feedback units per revolution value of the axis |
None |
|
|
Read following error in user units |
None |
|
|
Returns the status of the internal generator of the axis |
DINT |
|
|
Get the value period of the axis |
None |
|
|
Read actual torque |
None |
|
|
Get the user units per revolution value of the axis |
None |
|
|
Read actual velocity |
None |
|
|
Checks if an axis is ready. Returns TRUE if the internal realignment axis is ready. |
BOOL |
|
|
Realigns the actual position with the reference position by moving the axis by the specified delta position |
BOOL |
|
|
Performs a relative move for a specified distance from the current position |
BOOL |
|
|
Clears errors of the specified axis |
BOOL |
|
|
Resets the Fast Input |
BOOL |
|
|
Returns the status of the axis |
DINT |
|
|
Stop with the specified deceleration |
None |
|
|
Returns the timestampA timestamp is a sequence of characters, denoting the date and/or time at which a certain event occurred of the triggered axis |
DINT |
|
|
Sets the value period of the axis |
BOOL |
|
|
Forces the pipe position internal value. This function is working only when no pipe is connected. |
BOOL |
|
|
Sets the logical zero position of an axis |
BOOL |
|
|
Sets the user units per revolution value of the axis |
BOOL |
|
Copyright © 2015 Kollmorgen™ |
|