VL.LIMITP

General Information

Type

NV Parameter

Description

Sets the velocity high limit; active in opmodes 1 (velocity) and 2 (position) only.

Units

Depends on UNIT.VROTARY or UNIT.VLINEAR

Rotary: rpm, rps, deg/s, custom units/s, rad/s

Linear: counts/s, mm/s, µm/s, custom units/s

Range

Range may be limited by ECCN 3A225 Limitations for Induction Motors (➜ p. 1)

Rotary:

0.000 to 15,000.000  rpm

0.000 to 250.000  rps

0.000 to 90,000.000 deg/s

0.000 to 1,250.000 custom units/s

0.000 to 1570.796 rad/s

Linear:

0.000 to 1,073,741,824,000.000 counts/s

0.000 to 250.000*MOTOR.PITCH mm/sec

0.000 to 250,000.000*MOTOR.PITCH µm/s

0.000 to 1,250.000 custom units/s

Default Value

Rotary:

3,000.000  rpm

50.000 rps

18,000.002 deg/s

250.000 (custom units)/s

314.159 rad/s

Linear:

0.050 counts/s

50.000*MOTOR.PITCH mm/sec

50,000.004*MOTOR.PITCH µm/sec

250.000 custom units/s

Data Type

Float

See Also

VL.LIMITN , VL.CMD

Start Version

M_01-00-00-000

Description

VL.LIMITP sets the velocity command positive limit.

If the input to the velocity loop is higher than VL.LIMITP, then the actual velocity command VL.CMD is limited by the value of VL.LIMITP.

Related Topics

1   Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™