AXIS#.SAFE.STO.REPORTFAULT
Description
This parameter controls whether a Safe Torque Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Off (STO) fault F9000 will be created when STO is activated while the axis is enabled. The STO warning W9000 is always generated if this parameter is 1 and the STO function is active.
Value |
Description |
---|---|
1 |
W9000 / F9000 are generated when axis is enabled and an STO occurs (default) |
0 |
W9000 / F9000 are not generated |
Context
For complete STO information refer to STO (Safe Torque Off).
For complete STO information refer to STO (Safe Torque Off).
Related safety parameters:
- AXIS#.SAFE.STO.A
- AXIS#.SAFE.STO.ACTIVE
- AXIS#.SAFE.STO.B
- AXIS#.SAFEPARAM.STO.RESTARTACKMODE
- AXIS#.SAFEPARAM.STO.RESTARTACKSOURCE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-00-00-000 |
|
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 or 1 |
Default Value |
1 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AXIS1.SAFE.STO.REPORTFAULT |
5007h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.SAFE.STO.REPORTFAULT |
5107h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.SAFE.STO.REPORTFAULT |
10003 |
2713 |
Unsigned8 |
Read/Write |
- |
AXIS2.SAFE.STO.REPORTFAULT |
75539 |
1271 |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.SAFE.STO.REPORTFAULT |
10003 |
Unsigned8 |
Read/Write |
- |