AXIS#.SAFEPARAM.SBC​.BRAKE#ATTACHED

Description

Indicates whether Safe Brake Control (SBC) is enabled on this axis. Axis 1 can have SBC enabled with two assigned brakes. Axis 2 can only have SBC enabled with one brake (ie: BRAKE2ATTACHED cannot be set).

Value Description

0

No brake configured

1

Brake attached – without SDB (brake is applied before STO occurs according to AXIS#.SAFEPARAM.SBC​.BRAKETIMEDELAY)

2

Brake attached – with SDB (brake is applied after STO occurs)

IfAXIS#.MOTOR.BRAKE and BRAKE#.AXIS indicates no brake is attached to the axis but this safety parameter indicates a brake is attached, a warning will occur.

It is allowed to have a brake configured on the axis without enabling SBC using AXIS#.MOTOR.BRAKE and BRAKE#.AXIS.

 

Parameters Editor with Encoder 3 (EnDat) options displayed and circled

Context

For complete SBC information refer to SBC (Safe Brake Control).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0, 1, 2

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.SAFEPARAM.SBC.BRAKE1ATTACHED

3156h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SBC.BRAKE2ATTACHED

3156h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SBC.BRAKE2ATTACHED

3256h

02h

Unsigned8

-

-

Read/Write

No