MLAxisFBackPos

Pipe Network motion icon

 Function - Returns the feedback position of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

No range

N/A

No default

ID Name of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

Position

LREAL

No range

User units

Returns the feedback position of the axis.

See Set the Axis Block Position Units.

Remarks

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Position := MLAxisFBackPos( PipeNetwork.Axis1 ) ;

See Also