MLAxisPipePos

Pipe Network motion icon

 Function - Returns the pipe position of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

-2147483648 to 2147483647

N/A

No default

ID Name of the Axis block.

Speed

LREAL

No range

User unit/sec

No default

Sets the axis speed.

See Set the Axis Block Position Units.

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

See Function - General Rules.

Position

LREAL

 

 

See Set the Axis Block Position Units.

Remarks

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Pipe_Position := MLAxisPipePos (PipeNetwork.Axis1 ) ;

See Also