MLAxisGenPos

Pipe Network motion icon

 Function - Returns the generator position of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

No range

N/A

No default

ID Name of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

See Function - General Rules.

Position

LREAL

 

 

Returns the Axis generator position value.

See Set the Axis Block Position Units.

Remarks

  • Returns TRUE if the internal generator axis is ready.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Generator_Position := MLAxisGenPos(PipeNetwork.Axis1 ) ;

See Also