Gear

Name

Description

MLGearInit

Initializes a Gear Pipe Block with user-defined settings and for use in a PLC program.

MLGearReadOffset

Returns the Offset value of a selected Gear Block from the Pipe Network.

MLGearReadOffSlp

Returns the Offset Slope value of a selected Gear Block from the Pipe Network.

MLGearReadRatio

Returns the Ratio value of a selected Gear Block from the Pipe Network.

MLGearReadRatSlp

Returns the Ratio Slope value of a selected Gear Block from the Pipe Network.

MLGearWriteOff

Sets the Offset value of a selected Gear Pipe Block.

MLGearWriteOSlp

Sets the Offset Slope value of a selected Gear Pipe Block.

MLGearWriteRatio

Sets the Ratio value of a selected Gear Pipe Block.

MLGearWriteRatSlp

Sets the Ratio Slope value of a selected Gear Pipe Block.

Examples of Gear Functions

The output value starts with offset = 0 and gain = 1 (blue line)

Call the MLGearWriteOff function to modify the Offset.

This is where Offset_Slope is set with the MLGearWriteOSlp function.

After setting the Offset (Q=TRUE in the previous figure), call the MLGearWriteRatio function to modify the gear Ratio.

This is where Gain_Slope is set with the MLGearWriteRatSlp function.

The output value is adapted with the gear offset and ratio (blue line).