Backup and Restore tab

The controller can backup and restore EtherCAT devices on an EtherCAT network.

This feature:

  • Is useful as a maintenance operation to replace any controller drives in an operational machine.
  • Reduces the manual steps for saving/loading each drive’s firmware and parameters into a few automated steps.

The Backup/Restore functionality is located in the controller's Web server and is accessible from a web browser.

See these topics for more information:

See the Controller Backup and Restore in the KAS-IDE help.