MC_MachRegist
Function Block- Enables Mark-to-Machine registration.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to enable registration. |
|
Axis |
AXIS_REF |
The range of .AXIS_NUM is [1, 256] |
N/A |
N/A |
Axis whose position is used to determine a good mark. |
|
TriggerInput |
TRIGGER_REF |
No range |
N/A |
No default |
Structure specifying the fast input. The structure elements are: DirectionINT Range = 1, 5.
InputID INT Range = 0 to 1
TrigIDINT Range = 0 to 256.
|
|
Distance |
LREAL |
|
User units |
N/A |
|
|
Tolerance |
LREAL |
When converted to feedback units, |
User units |
N/A |
This value specifies the distance, plus or minus, about Distance to determine if the mark detected by the fast input is a good mark. |
|
Ignore |
LREAL |
|
User units |
N/A |
This value specifies the distance after the previous good mark in which any detected marks are ignored. |
|
Target |
LREAL |
When converted to feedback units,
|
User units |
N/A |
|
|
Position |
LREAL |
When converted to feedback units,
|
User units |
N/A |
|
|
PosAxis |
AXIS_REF |
The range of .AXIS_NUM is [1, 256] |
N/A |
N/A |
The position of this axis at the time the fast input occurs is compared to the Target position. This comparison determines the amount of registration compensation to apply. |
|
CompAxis |
AXIS_REF |
The range of .AXIS_NUM is [1, 256] |
N/A |
N/A |
The calculated registration compensation is applied to this axis. |
|
PosTolerance |
LREAL |
When converted to feedback units, the range is [-251, 251-1]. |
User units |
N/A |
This value specifies the distance, plus or minus, about the Target position to determine if the position is accepted and the compensation value is calculated and applied. |
|
RatioNumerator |
DINT |
When converted to feedback units, |
User units |
N/A |
|
|
RatioDenominator |
DINT |
When converted to feedback units, |
User units |
N/A |
|
|
Options |
UINT |
See the MC_MachRegist Options Table. |
N/A |
N/A |
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
RegistOn |
BOOL |
FALSE, TRUE |
N/A |
Indicates registration is activated. |
|
Aborted |
BOOL |
FALSE, TRUE |
N/A |
Indicates registration has been terminated by MC_StopRegist. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
Indicates an invalid input was specified or the registration was terminated due to an error. |
|
ErrorID |
INT |
No range |
N/A |
|
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
If using a dual-core controller, see Call Function Blocks Multiple Times in the Same Cycle.
-
- Is this the right function block to use?
See Decide which Function Blocks to Use for Registration and Registration Application Guide.
- It is used on any servo or digitizing axis and with any move type.
- It is used most frequently in master/slave applications.
|
Used with ... |
Effect |
|---|---|
|
Non-slave moves |
Resets the axis position when a good mark is captured by the fast input. |
|
Slave moves |
Applies a compensation offset to correct for the difference between the target position and the measured position. This provides the ability to compensate for product or process inconsistencies, provides a system that remains synchronized with no accumulated error, and maintains repeatable accuracy throughout the process. |
Transition and Registration
- A positive transition of the En input starts registration.
- The application may change the registration parameters while registration is active by changing the input values and causing another positive transition of the En input.
- The function block then reads and applies the new values.
- The axis number at the Axis input indicates the axis whose position, at the fast input, is used to determine if the mark is a good mark.
Distance, Tolerance, Ignore, Target Inputs
- The Distance, Tolerance, and Ignore inputs are used to determine whether or not the registration mark is good.
- For a mark to be recognized as good, it must be outside of the Ignore distance and the correct Distance from the previous mark +/- the Tolerance window.
- A mark is bad if it occurs outside of the “good tolerance band” and is not ignored.
- Both good marks and bad marks are recognized as marks, ignored marks are not recognized.
- If all marks are to be recognized as good marks, enter 0 (zero) at both Distance and Tolerance.
- The Distance value defines the distance between good marks.
- In Clear Lane and Product registration the Distance input value is typically the same as the Target input value.
- In Print registration, the Distance is typically not the same as Target.
- The Tolerance value is the distance, plus and minus, about Distance.
- Marks detected in this window are good marks and registration occurs.
- Marks detected outside this window and outside the Ignore band, are bad marks and registration does not occur.
- This window should be large enough to allow for the worst case error in the distance between the previous mark and the current mark.
- The Ignore value defines the distance from the previous mark where all marks detected by the fast input are ignored.
- This is crucial when registering products that do not have Clear Lane registration marks.
- The Target input is the expected target position that is used to calculate how much registration compensation is to be applied when a registration mark is considered good.
- When a good mark is detected, the position of the PosAxis is compared to the Target position to calculate a correction.
- The registration correction is only applied with master/slave move types.
Position and Option Inputs
- The Position input is the position value the registration Axis position is reset to when a good registration mark is detected.
- When a good mark occurs, the position of the PosAxis is compared to the Target position.
- This comparison is used to calculate the amount of registration compensation to apply to the CompAxis.
- Registration compensation is applied to the axis specified at the CompAxis input under these conditions:
- If CompAxis is a master axis, the compensation is applied to the master offsets of all its slaves.
- This shifts the master’s position as seen by its slaves.
- If CompAxis is executing a slave move (e.g., MC_GearIn or MC_CamIn), the compensation is applied directly to the axis.
- This comparison is used to calculate the amount of registration compensation to apply to the CompAxis.
- The PosTolerance input is the distance, plus and minus, about the Target position used to determine if compensation is applied.
- When a good mark occurs, the position of the PosAxis axis is checked to see if it lies in the window defined by PosTolerance.
- If it is in the window, compensation is applied.
- If it is outside the window, compensation is not applied even though a good mark was found.
- When a good mark occurs, the position of the PosAxis axis is checked to see if it lies in the window defined by PosTolerance.
- If PosAxis and CompAxis are different axes, the RatioNumerator and RatioDenominator inputs define the conversion factor for calculating the compensation value.
- This is needed because the amount of error between actual and target positions is determined by the PosAxis's position and the compensation is applied to the CompAxis.
- The RatioNumerator should typically be the number of User Units of CompAxis motion for one registration cycle.
- The RatioDenominator should typically be the number of User Units of PosAxis motion for one registration cycle.
- If PosAxis and CompAxis are the same, RatioNumerator and RatioDenominator should be the same value, thus resulting in a 1:1 ratio.
- When a good mark occurs, the position of the PosAxis is compared to the Target position.
- The Option input defines various modes of operation for registration.
- The first bit, 0001H, selects Absolute or Resetting.
- This refers to the way the second mark and all subsequent marks are determined to be good marks.
- With both registration schemes, the very first detected mark is the starting point.
- With Resetting registration, when the next mark is detected, the position of that mark becomes the starting point for the next good mark detection calculation and so on.
- The starting point is reset with each good or bad mark.
- This allows the product to re-synchronize, if necessary, due to process issues (e.g., product shift) etc.
- Absolute registration determines all good marks based on the very first mark.
- The position of the second and each subsequent mark is compared to an integer multiple of Distance from the very first mark.
- This method insures the product always registers to a known fixed distance.
- The starting point is reset with each good or bad mark.
- The third bit, 0004H, must be 0 (zero).
- Mark-to-machine registration requires time-based capture.
- The first bit, 0001H, selects Absolute or Resetting.
Figure 1: MC_MachRegist
MC_MachRegist Options Table
|
Hexadecimal |
Decimal |
Option |
Description |
|---|---|---|---|
|
0001 H |
1 |
Absolute/Resetting |
0 = Resetting, 1 = Absolute |
|
0002 H |
2 |
Reserved |
0 |
|
0004 H |
4 |
Time/position based capture |
0 = time based capture, 1 = position based capture |
|
0008 H |
8 |
Inhibit Reference on Good Mark |
0 = Perform reference, 1 = inhibit reference When this bit is set, the Position function block argument is unused and the axis position is not changed when a registration mark is encountered. |
|
0010H |
16 |
Inhibit Master Compensation |
0 = Perform Master Compensation, 1 = Inhibit Master Compensation |
|
0020H |
32 |
Inhibit Slave Compensation |
0 = Perform Slave Compensation, 1 = Inhibit Slave Compensation. |
-
-
To use Capture Engine 1, modify the input PDOs that are used and add the Latch Position 1 parameter.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_MC_MachRegist( ActivateReg, Axist2, Trig1, 360, 5, 90, 180, 0, Axis2, Axis2, 10, 1, 1, 0 );
See Also