RxPDO - AKD Drive CANopen Objects
This table identifies:
- The CANopen objects required by the motion engine and function blocks.
- Whether the objects are available in the default PDO.
- Their corresponding drive parameter.
-
-
Review the table to verify the objects needed by the features the application uses are included in the PDO selection.
|
Index - subindex |
Object Name |
Required |
Associated ML FB |
Associated MC FB |
Associated Drive Parameter |
|---|---|---|---|---|---|
|
0x20A4 - 0 or 0x2802 - 0 |
Latch control word |
No |
|
|
|
|
0x3470 - 3 |
AOUT.VALUE Used by Onboard I/O mappings |
No |
N/A |
N/A |
|
|
0x6040 - 0 |
|
Yes |
|
|
|
|
Additive torque value Torque Feed Forward |
No |
|
N/A |
|
|
|
0x60C1 - 1 |
Position demand value |
Yes |
|
|
|
|
0x60FE - 1 |
Digital outputs Used by Onboard I/O mappings |
No |
N/A |
N/A |
|