RecipeClose

This function/function block was added in KAS 5.00.

PLCopen motion icon Pipe Network motion icon

 Function Block - Close a recipe object.

RecipeClose unloads a recipe object from the actively running program.

  • RecipeClose does not delete the recipe file used to create the recipe object.
    • To delete a recipe file, use the FileDelete function block.
  • RecipeClose does not save changes made to the recipe object.
  • If instances were modified via RecipeStoreInstance, call RecipeSave before to persist the changes to the file system.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, close the specified recipe object.

RecipeID

UDINT

No range

N/A

No default

  • The ID of the recipe object to close.
  • RecipeID is the handle ID returned by the RecipeOpen function block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Busy

BOOL

FALSE, TRUE

N/A

If TRUE, the function block is executing.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

Enumerated

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Inst_RecipeClose(True, recipeID);
IF Inst_RecipeClose.Error THEN
   errorMessage := MC_ErrorDescription(Inst_RecipeClose.ErrorID);
END_IF;

See Also