RecipeSave
This function/function block was added in KAS 5.00.
Function Block - Save a recipe object to a file.
- RecipeSave writes the recipe object (definition + stored instances) to the filesystem.
- It does not read live PLC values.
- To capture PLC values before saving, call RecipeStoreInstance beforehand.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, save the recipe to the file RecipeFile. |
||||||
|
RecipeID |
UDINT |
No range |
N/A |
No default |
|
||||||
|
RecipeFile |
STRING |
No range |
N/A |
No default |
The path of the destination recipe file. |
||||||
|
RecipeFormat |
SINT |
Enumerated |
N/A |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
Enumerated |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_RecipeSave(True, recipeID, 'Parts_Recipes.xml', RCP_FMT_XML); IF Inst_RecipeSave.Error THEN errorMessage := MC_ErrorDescription(Inst_RecipeSave.ErrorID); END_IF;
See Also