RecipeStoreInstance
This function/function block was added in KAS 5.00.
Function Block - Store the present values of the program data in a recipe instance.
- If an instance with the specified name already exists, the values in that instance are overwritten.
- If no instance exists with the specified name, a new instance with the specified name is created.
- No range validation is performed while storing.
- Validation is deferred until a later call to RecipeApplyInstance.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, save the program data into the named recipe instance. |
|
RecipeID |
UDINT |
No range |
N/A |
No default |
|
|
Name |
STRING |
No range |
N/A |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
Enumerated |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_RecipeStoreInstance(True, recipeID, 'Cogs');
IF Inst_RecipeStoreInstance.Error THEN errorMessage := MC_ErrorDescription(Inst_RecipeStoreInstance.ErrorID); END_IF;
See Also