RecipeOpen

This function/function block was added in KAS 5.00.

PLCopen motion icon Pipe Network motion icon

 Function Block - Open a recipe file and create a recipe object.

Recipe files opened with RecipeOpen must include a recipe definition section.

  • Instance sections are optional.
  • Recipes without instance sections can be opened and used later with RecipeStoreInstance to create instances from active program data.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, load a recipe file.

RecipeFile

STRING

No range

N/A

No default

The location of the recipe file.

RecipeFormat

SINT

Enumerated

N/A

No default

  • The recipe file format.
  • Valid values include one of these enumeration values:

Value

Description

RCP_FMT_XML

XML file format.

RCP_FMT_TOML

TOML file format.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Busy

BOOL

FALSE, TRUE

N/A

If TRUE, the function block is executing.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

Enumerated

N/A

RecipeID

UDINT

No range

N/A

The ID of the recipe object.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Inst_RecipeOpen(True, 'Parts.xml', RCP_FMT_XML);
IF Inst_RecipeOpen.Error THEN 
   errorMessage := MC_ErrorDescription(Inst_RecipeOpen.ErrorID); 
ELSE 
   recipeID = Inst_RecipeOpen.RecipeID 
END_IF; 
//                         Inst_RecipeOpen(True, '/usbflash/recipes/Parts.xml', RCP_FMT_XML); IF Inst_RecipeOpen.Error THEN    errorMessage := MC_ErrorDescription(Inst_RecipeOpen.ErrorID); ELSE    recipeID = Inst_RecipeOpen.RecipeID END_IF;

See Also