MT.CONTINUE

Description

MT.CONTINUE continues a motion task that has been stopped by the DRV.STOP command.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

0

Data Type

N/A

See Also

MT.NUM, MT.P, MT.V, MT.CNTL, MT.ACCMT.V, MT.DEC, MT.TNUM, MT.MTNEXT MT.MTNEXT, MT.SET , MT.LOAD

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2267 Command* No
Sercos® III

*For PROFINET, write a value of 0 into the PNU to execute a command.

EtherNet/IP
Instance Data Size Data Type
268 Command None
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

534

No Command No M_01-03-00-000

Related Topics

Motion Tasks