KAS Application tab
Usage
This tab is used to:
- Display general information about the currently loaded project on the controller.
- Start and stop the motion.
- Display the Axes run by the controller from the Axis sub-tab.
- Manage log messages from the Log Configuration tab and Log Data tab.
- Display User Data present on the controller from the User Data tab.
- Connect to a remote computer from the Shared Directory tab.
- Open the web-based Control Panels using the Diagnostic Panels sub-tab.
|
Item |
Description |
|---|---|
|
Version of KAS App |
This label provides information about the name and version number of the application that is in the controller.
|
|
Status of KAS App |
The state of the application, either: Started or Stopped. |
|
Start |
|
|
Cold Start |
|
|
Stop |
Stop the application. |
|
Auto-start |
Select this option to automatically start the KAS application when the controller is powered up.
|
|
Clear all errors |
Click this button to clear the error log for all axes. |