You are here: Using the PDMM or PCMM Controller > Working with the Hardware > EtherCAT Devices Backup and Restore > EtherCAT Devices Backup

EtherCAT Devices Backup

The Backup operation discovers all the devices on the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network and stores the topology information, AKD firmware files, and AKD parameters to the controller’s local storage.

Controller Local Storage
PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system Compact Flash Card
PDMM or PCMM SD Memory Card (see SD Card Support for more information)

Before starting a backup of the EtherCAT Devices, you will need:

Backup Steps

  1. From the web server home page, click on the Backup & Restore tab:
  2. Under the Backup tab, press the Backup EtherCAT Devices button.

    The web server will ask you to choose a firmware package file and suggest the filename that matches the firmware version on your drives. Selecting the firmware package file is a one-time event. The controller will remember your selection and will not ask you again for future backups.

  3. Press the Continue Backup EtherCAT Devices button. It will take a couple of minutes or longer, depending on the number of AKDs in the system.

When the backup is complete, the web server will indicate whether the backup was successful.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™