AXIS#.SAFE.STO.REPORTFAULT

Description

This parameter controls whether a Safe TorqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Off (STO) fault F9000 will be created when STO is activated while the axis is enabled. The STO warning W9000 is always generated if this parameter is 1 and the STO function is active.

Value

Description

1

W9000 / F9000 are generated when axis is enabled and an STO occurs (default)

0

W9000 / F9000 are not generated

Context

For complete STO information refer to STO (Safe Torque Off).

For complete STO information refer to STO (Safe Torque Off).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 or 1

Default Value

1

Data Type

Integer

Stored in Non Volatile Memory

Yes